Ribbon button text gets truncated

2021-10-06T23:27:52Z

Summary


Details

The icon button text to be added by File > Customize function as New User Command, is different from UGII_LANG=English and UGII_LANG=japanese on showing double-bytes. The last a few characters are missing only on UGII_LANG=japanese.

Step to reproduce: 
1.File > Customize ( or Ctrl+1)
2.Add New Item like New User Command to ribbon bar
3.Edit the button text to be displayed in two lines ( with 6 or more Japanese characters)



Solution

The issue is fixed in NX1980.


Work around:
Add a double-byte( or two single-byte) space character at the end of the string.
or
If it's UGII_LANG = English, no problem happens and works well.



Notes and References

In NX12 or before release, the behavior was completely the same. It has changed since NX1847 release.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1926
Function: UI_TOOLS

Ref: 002-8525113

KB Article ID# PL8525113

Contents

SummaryDetails

Associated Components