Behavior changes to the view scale applied after executing "Reset Orientation"/"Reset View Orientation"

2021-10-06T23:27:52Z

Summary


Details

When executing "Reset View" or "Reset View Orientation", "Saved View Scale" is applied even though "Fit" is specified in "Orient View" or Customer Default.

Step to reproduce: 
1.Make sure to set "Fit" as "View Scale" in Gateway > Display > Miscellaneous.
2.Open a .prt which has the state with saved view scale.
3.In PNT, select a "Model View" > MB3 > "Reset Orientation"

The behavior in NX1847 or before:
The behavior in NX1872 or later:




Solution

The issue has been fixed in NX1872.


Work Around:
 Making use of "Fit"(Ctrl+F) explicitly  if you would like to have "Fit"  for all objects

Notes and References

There was a difference on the behavior depending on the function in NX 1847 Series or before(including NX12, NX11 or before). The changes have been applied to unify the behavior on the view scale applied after command.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V1872
Function: VIEW_SAVE

Ref: 002-8525111

KB Article ID# PL8525111

Contents

SummaryDetails

Associated Components