Unable to open JT file in NX

2021-10-06T23:27:52Z

Summary


Details

When trying to open exported JT file, the problem occurs only if the default name of Model Reference Set in Customer Default is set to null(blank).


Step to reproduce: 
1.Start NX > Customer Default > Assemblies > Site Standard > Reference Sets > Model Reference Set, set "Name" input field to blank(null).
2.Restart NX > open a new part and put a solid like a box.
3.File > Export > JT ( with default setting)
4.File > Open > select the exported JT file.



Solution

The problem is fixed in NX1980.

Work Around:
It's only one way to work around the issue. The input field for "Model Reference Set" in Customer Default must set some input value like "MODEL", "Ref#1" or etc...

Notes and References

The exported data by Export JT has no problem and is reliable. Problem is just on Open > JT.


The issue does not occur in NX1872 or before release, but it occurs in NX1899 Series or later.
In addition, even JT file is not generated in NX1953.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V1934
Function: OPEN_JT

Ref: 002-8525110

KB Article ID# PL8525110

Contents

SummaryDetails

Associated Components