While trying to upload NX templates showing error

2021-10-06T23:27:52Z

Summary


Details

Error: (720100) - Failed to initialize log file for clone operation. 
 While performing import 
***** ug_clone import operation failed


Received this message while importing templates using tcin_template_setup.bat 



Solution

The issue was resolved with the below two changes to the command prompt and these helped to import the templates successfully.


Set the variable: UGII_TMP_DIR=c:\temp 
Running the command from C:\temp location instead of NX install location where we have full write permission. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1953
Function: CLONE_IMPORT

Ref: 001-9982360

KB Article ID# PL8525049

Contents

SummaryDetails

Associated Components