Solid Edge Recommended versions of Windows 10 for SE2021

2021-10-06T23:58:03Z
PART/SHEETMETAL

Summary


Details

What are the current recommended versions of Windows 10 for Solid Edge 2021?



Solution

All versions of Windows 10 (Professional and higher editions) that are currently in the active servicing timeline provided by Microsoft (https://docs.microsoft.com/en-us/windows/release-health/release-information) are supported with Solid Edge 2021.
 
Our recommendation has always been that customers should delay taking Windows 10 Feature Updates (new versions/operating systems) for as long as possible (https://support.sw.siemens.com/knowledge-base/PL8008188).  This is because we believe that maturer Windows 10 versions provide for more overall stability than newer recently released Windows 10 versions.

 As the maturest Windows 10 version approaches end of servicing with Microsoft we would then recommend that customers begin migrating over to the next maturest Windows 10 version that is actively supported by Microsoft.
 
As such, at this time, we recommend that customers should be using Windows 10 version 1909 as it is the most mature actively supported version of Windows 10.  As 1909 approaches end of servicing with Microsoft we would then recommend customers begin migrating over to the next maturest supported version of Windows 10 which is currently version 2004.




Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: SETUP
Version: V221.0
Function: INSTALL

Ref: 001-9980797

KB Article ID# PL8524837

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES