Cannot get NX to work with Solid Edge/NX license bundle
2021-10-06T23:58:03Z
Summary
Details
Able to get Solid Edge licensed and running with the Solid Edge/NX license bundle, but cannot get NX to work. Are there additional steps required to get NX to run?
Solution
Yes, there are additional steps required to license the NX side of the bundle. The first step is go to the NX Licensing Tool that is located in your Start menu.
Once inside the NX Licensing Tool, the Bundle you have will need to be selected and added. In this particular case NX CAD/CAM 3 Axis Milling is the Available Bundle. Select it, then add it. It will then be listed in Applied Bundles.
Apply the change. You will then be able to start your NX product.