SolidWorks Data Migration aborts with an error 0xFFFFFFFF800706BE while processing a drawing file

2021-10-06T23:58:02Z

Summary


Details

The scenario here the SolidWorks Data Migration aborts whenever a drawing file will be processed. Part and assembly files on the other hand can be processed without any problem.

The process of migrating a drawing file (e.g. Assem1.SLDDRW) ends with the following error:

Processing File D:\workdir\sw\Assem1.SLDDRW 
The SolidWorks file D:\workdir\sw\Assem1.SLDDRW will be extracted as D:\workdir\se\Temp\Assem1.dxf 
  D:\workdir\sw\Assem1.SLDDRW  Error :   0xFFFFFFFF800706BE

Solution

Try the following steps to resolve this issue:

- Start SolidWorks.
- Create a new drawing.
- Open the 'Options' dialog.
- Select the 'System Options' tab.
- Select 'Export' area.
- Set the 'File Format' to 'DXF/DWG'.
- Find the section 'Custom Map SOLIDWORKS to DXF/DWG'.
- Deactivate the 'Enable' option within this section.
- Confirm the new settings with OK.
- Close the drawing without saving.
- Exit SolidWorks.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V221.0
Function: SW

Ref: 002-8524815

KB Article ID# PL8524815

Contents

SummaryDetails

Associated Components