Solid Edge How to remove ghost parts in an assembly document which has Pattern components?

2021-10-06T23:58:01Z
ASSEMBLY

Summary


Details

A user locates some questionable Pattern components that are visible in the active window of an opened assembly document, but which are not assigned to an equivalent component in the structure of the PathFinder. Components like these are often called ghost parts.

Solution

Use the following steps to remove these ghost parts:

- Close the assembly document with the ghost parts issue.
- Exit Solid Edge.
- Run Registry Editor.
- Open Computer\HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version 221\DEBUG
- Choose Edit > New > DWORD (32-bit) Value.
- Enter Value name: ALLOW_PATTERN_FIXUP
- Select the new value > Right-Click > Modify...
- Enter Value data: 1
- Choose OK.
- Minimize Registry Editor.
- Start Solid Edge.
- Open the assembly document with the ghost parts issue.
- Notice that the ghost parts are now not visible anymore in the active window.
- Save the assembly document (if the ghost parts are still visible do not save the file).
- Close the assembly document.
- Exit Solid Edge.
- Return to the Registry Editor.
- Return to Computer\HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version 221\DEBUG
- Select the value ALLOW_PATTERN_FIXUP > Right-Click > Delete
- Confirm the deletion of the value with Yes
- Close the Registry Editor.
- Start Solid Edge again.
- Open the assembly document in question again.
- Notice that the ghost parts issue is solved.

Notes and References

If the above steps do not solve the issue please check whether one of the following value names help instead:

- ALLOW_BC_FIXUP > removes ghost parts in assembly files which has Fastener system components
- ALLOW_PIPE_FIXUP > removes ghost parts in assembly files which has XpresRoute components

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V221.0
Function: COMPONENTS

Ref: 002-8524579

KB Article ID# PL8524579

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS