Details
A customer has Solid Edge Technical Publications ST10 installed on several workstations and asks for a command line to silently uninstall this installed version in preparation to install a newer version.
Solution
This task can be accomplished by using the following command line from an Administrator Command Prompt:
"C:\Program Files\Solid Edge Technical Publications\UNWISE.EXE" /A /S "C:\Program Files\Solid Edge Technical Publications\INSTALL.LOG"
Note: The default folder location (C:\Program Files\Solid Edge Technical Publications) should be adjusted to match the customer environment .
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V110.0
Function: INSTALL
Ref: 002-8524571