NX How to relax tangent relation in sketch (NX1953)?

2021-10-06T23:27:52Z
NX for Design

Summary


Details

Unable to relax tangent relation in the new Sketch.

How do we relax the tangent relation on the right side of the image? So that we can get a "non-tangent" connection


Solution


The fillet relation is not shown to the user because it would clutter the screen with many symbols that he will never relax.
So we made fillet (a bitangent arc) no relax-able.


There are many ways to change the fillet to a non-fillet. One of them is shake to detach and then make corner.

Example:

To do this, select the line at the upper end and then shake the mouse with the left mouse button ( MB1) held down. This will detach the line and it can then be trimmed or tied to the upper radius.

Step 1 
Step 2

Step 3
the result :


Notes and References

9975082 




Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1946.3400
Function: SKETCHER

Ref: 002-8524474

KB Article ID# PL8524474

Contents

SummaryDetails

Associated Components

Modeling