How to Install Solid Edge 2021 CAMPro.

2021-10-06T23:58:00Z

Summary


Details

How to Install Solid Edge 2021 CAMPro.

Solution

1. Go to the Support Center:  https://support.sw.siemens.com/en-US
2. Click on 'Downloads'.
3. Click on 'Solid Edge 2021 Portfolio.
 

4. Click on 'CAMPro' and click on 'Solid_Edge_SECAMPro_2021_1938.exe' to download it.
 



5. Click on 'Solid Edge 2021 Portfolio. This is to get 'plmxmlAdapterSE70.dll' which you will need to replace the one in '%UGII_BASE_DIR\NXBIN\'
 

 
 
6. Click on 'PLMXML' and click on 'V221_PLMXML_FILES.zip'.
 

 
7.  Unzip this file to get 'V221_PLMXML_FILE\V221\VS2017\64Bit\plmxmlAdapterSE70.dll'. Backup %UGII_BASE_DIR\NXBIN\plmxmlAdapterSE70.dll' delivered with NX and copy the new one to this location. Solid Edge 2021 files should be able to open in NX at this point. If you try to open Solid Edge 2021 files in Solid Edge CAMPro without replacing the plmxmlAdapterSE70.dll, you will get an 'Open' error ('The part file is from a newer version of the application than the one supported by NX').

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: SE_CAM_PRO
Version: V221.0
Function: INSTALL

Ref: 002-8524473

KB Article ID# PL8524473

Contents

SummaryDetails

Associated Components