SEDM has no folders to select in the indexing tool

2021-10-06T23:58:00Z

Summary


Details

In a client - server configuration for Solid Edge Built-in Data Management (SEDM) the user is unable to select an index location in the Indexing options utility.  The Indexed Locations are empty:
 


Solution

In this instance, the user is running the Remote Desktop Session Host (RDSH) role on their server.  This role has a known limitation in that it will disable Windows search.

https://docs.microsoft.com/en-US/troubleshoot/windows-server/shell-experience/windows-search-is-disabled-by-default

By default, the Windows Search service is set to Disabled in Windows Server 2016.  This is because indexing of the volumes can cause problems in certain scenarios, such as with Cluster Shared Volumes (CSV) and in running Remote Desktop Session Host (RDSH) with multiple simultaneous sessions.

Currently there is no option to enable Windows search with the RDSH role enabled.  Since Windows search is required to run SEDM this configuration is not supported.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 2019
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEDM

Ref: 002-8524470

KB Article ID# PL8524470

Contents

SummaryDetails

Associated Components