NX Benefit of Mechanical Routing templates

2021-10-06T23:27:51Z
NX for Design

Summary


Details

Is there a benefit to using the Routing templates in the NX 'File New' dialog? 
Or can the Model templates be used and then switch to the Routing application? 



Solution

The benefit for using the Routing templates is minimal. 
The Model templates can be used and then switch to the Routing application. 
The idea of the Routing templates is to take the user directly to the Routing application when the user is creating a new file. But the Routing templates do not have anything within them that sets them apart from the Modeling templates other than some minor preference settings (preference of the ECAD data type to import as an example). 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1847
Function: FILE_NEW

Ref: 001-9972969

KB Article ID# PL8524113

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX