Solid Edge Assembly simplification modeling reverts to mm

2021-10-06T23:57:59Z
ASSEMBLY

Summary


Details

When creating an enclosure in Assembly Simplification, if the default templates have different units than the assembly itself, then the units will not be the same. In other words, if the assembly was created using ANSI inch and the default templates are metric, when you add an enclosure the units will be mm. 



Solution

In Solid Edge Options, under Helpers, select "Set Default Templates". Change the default templates so the units are the same as the active assembly. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V221MP2
Function: SIMPLIFY

Ref: 001-9971179

KB Article ID# PL8524109

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS