Failed to open STEP file directly from MS Outlook

2021-10-06T23:57:59Z

Summary


Details

Opening a STEP file directly from MS Outlook failed with the message:

"Cannot save a document to Internet Cache location. Select the folder again to save the document."  

Solution

Check in the settings file "step.ini" (located in the Solid Edge installation folder e.g.  C:\Program Files\Siemens\Solid Edge 2021\Preferences\Translators) if the setting "Import Enable Default Output Path=" is set ON.
Change the Value to "OFF" and save the file.

The Step file should now be translated and opened in Solid Edge with the selected Solid Edge template directly from MS Outlook.








Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220MP11
Function: STEP

Ref: 002-8523994

KB Article ID# PL8523994

Contents

SummaryDetails

Associated Components