I cannot copy a sketch from one layer to another in the Solid Edge Draft environment.
Steps to reproduce:
Create a drawing.
Define two layers.
Make the first layer active and sketch some geometry.
Select the sketch and 'Copy'.
Make the second layer active and 'Paste'.
'Show only' the second layer - the pasted sketch is not there.
'Show only' the first layer - the sketch has been copied to this source layer.
Solution
Layers are not a place in which objects reside - they are merely display filters.
When you copy and paste, the new objects will retain the layer of the original objects - they will not obtain a different layer. Making a different layer the active layer before pasting will make no difference to this.
The workaround is to take the copied/pasted sketch from the source layer and use the Move Elements command that will move the selected geometry to another layer.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: n/a Product: SOLID_EDGE Application: DRAFT Version: V221.0 Function: LAYERS