End of Standard Maintenance for NX 1953 Series (Dec 2020) is listed below. This date represents when no further updates or fixes will be issued for the corresponding NX 1953 Series (Dec 2020). PLMS will continue to provide telephone support and assistance for NX. PLMS will attempt to duplicate any possible code defects on the revision of software the defect is reported (when available) and on the current release or revision of the product. PLMS will not write a PR unless the problem can be duplicated in a supported version of the product. If it is found that the defect does not occur in the latest revision of the software, the customer will be asked to update their product to the current revision to correct the problem.
Sincerely, Siemens Digital Industries Software SFB-NX-8523951 Product Information: