Some of circles cannot be plotted by SDI.

2022-06-23T01:47:30Z

Summary


Details

When plotting drawing sheet using HPGL2 format in SDI Plot, circle geometries are randomly missed and not output.

Reproduced Step:
1. Make sure to define HPGL2 format in UGII_SDI_SERVER_CFG_DIR.
2. Open any drawing part which Circles are included.
3. Select File-> Plot.
    Type: Standard
    Source: (Any drawing sheet/size that circles are input.)
    Printer-> (any HPGL2 format to be defined)
    Profile-> "System Profile"
4. Select "Advanced Plot" in "Actions".
5. Make sure that following are set.
    Printer Tab: Printer and Profile are set as the step "3." above.
    Print Setup Tab: Paper-> any sizes.
    Print Layout Tab: "Landscape" as "Orientation".
6. Print


KB Article ID# PL8523943

Contents

SummaryDetails

Associated Components