Synchronizing the Solid Edge Assembly Mass (Weight) to Teamcenter
2021-10-06T23:57:55Z
Summary
Details
In Solid Edge the Mass is a special attribute that requires some extra attention.
· Mass is a CAD driven property (/master=cad) · For Solid Edge Part and Sheet Metal files Mass is driven by the Material table (Material.mtl) · Since an assembly only contains a collection of parts you do not define a material at the assembly level. This results in that an assembly has no physical properties. · The calculated "Assembly Mass" is the summary of the mass of all parts.
To synchronize the Mass to Teamcenter you can map the Solid Edge property "Mass" to a Teamcenter property as shown in the attribute mapping example, below:
This mapping will not work for Dataset type = "SE Assembly".
The workaround is to expose the Mass property in the variable table in Solid Edge and map this exposed variable to a Teamcenter property. Best practice is to expose the Mass property on the managed template. You can then map the Mass for the SE Assembly:
· Create two parts with a material assigned, save to Teamcenter. · Create an assembly of these two parts, save to Teamcenter. · Using the Physical Property manager calculate the assembly Mass.
· Open the variable table and use the filter to show the Physical Properties
· In the Variable table expose the Mass attribute · Upload the assembly -> now it will sync the Mass with Teamcenter.
Remark:
Assembly mass will not update automatically during save. Keep in mind that you need to update the assembly mass manually. To perform this, open the Physical Properties Manager and click "Update all".
Hardware/Software Configuration
Platform: na OS: n/a OS Version: n/a Product: SOLID_EDGE Application: DOC_MANAGEMENT Version: V221.0 Function: SEEC