Problem creating multiple Part Boundaries with Specified Plane

2021-10-06T23:27:51Z

Summary


Details

When creating Part Boundaries with Plane set to 'Specify', only the first boundary is created on the specified plane.


Solution

The problem is fixed in NX 1953.

As a workaround in NX 1946, create the additional part boundary sets. These will not initially be created on the specified plane.

Select the incorrect boundary sets, and click on 'Inferred'. This will then move the boundary sets to the correct plane.


KB Article ID# PL8523687

Contents

SummaryDetails

Associated Components