Dialog Boxes - Not Being Remembered (Transformations CSYS To CSYS)

2021-10-06T23:27:51Z

Summary


Details

The "Tranformations" dialog box automatically selects the "Absolute" CSYS position when transforming "CSYS to CSYS" using "Dynamic" selection. Note..."Specify From CSYS" is preselected. (Please see image below).
Note: "Specify From CSYS" is preselected.

Solution

Change the selection to "Inferred" and the dialog memory will be as desired. See steps below...
  • Select the operation or operations with MB3.
  • Select Object - Transform (please see image below).
  • Change the "Transformation Parameters" to "Inferred" for both the following.
    • "Specify From CSYS"
    • "Specify To CSYS"
The dialog box will now be setup to allow you to select "CSYS" in your session.

Note: Further explanation of "CSYS dialog box" can be found by navigating to the link below...

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200507135732916.coord_sys_datums/html/com_tool_com_csyscon_d

Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1953
Function: USER_INTERFACE

Ref: 001-9968231

KB Article ID# PL8523617

Contents

SummaryDetails

Associated Components