NX Resistance spot welds are not getting Published to Teamcenter

2021-10-06T23:27:51Z
NX for Design

Summary


Details

Welds are not being published to Teamcenter. 



Solution

Make sure the welds are not in an assembly part. Welds will only be published in Teamcenter if they exist in a component part. 
In order for the welds to get published, you need to create a new empty component then make it the work part and create welds in this component. 
Make sure you use 'File-->Save-->Force Save All'. The welds won't get published if the welds are created at an assembly level. They have to be created in a component part. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1953
Function: FILE_SAVE

Ref: 001-3059044

KB Article ID# PL8523372

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX