Changing a large group of operations to explorer style dialog

2021-10-06T23:27:50Z

Summary


Details

Changing a large group of operations to explorer style dialog

Solution

The OOTB template operations were not totally updated to the "Explorer Format" until NX1926. In NX1926 and above, the customer can convert their operations to the "Explorer Format" by referencing the OOTB templates by doing the following...


  • Select all the operations that need to be converted.
  • MB3 on the selection.
  • Select Object-->Customize from..
  • "Copy Customization From" - "Objects in" -->"Template" -- Select OK (Please see image below).



For Versions Prior to NX1926 (if the customer wants to convert to the Explorer Dialog format).



It's suggested the OOTB template parts be converted to the "Explorer Dialog" format and the above method can be used to update all operations as needed.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1872
Function: TEMPLATES

Ref: 002-8523031

KB Article ID# PL8523031

Contents

SummaryDetails

Associated Components