Details
Always a default thread taper angle of 3.0 degrees for all thread standards is displayed in the drafting views.
How to customize this default thread angle to confirm different thread standards in the machinery handbook?
Solution
The default thread taper angle shown on drawing views is customized using the below environment variable.
UGII_NOMINAL_DRAWING_THREAD_TAPER_ANGLE
Set something like UGII_NOMINAL_DRAWING_THREAD_TAPER_ANGLE=1.783
Drafting views will be tapered by an angle approximately equal to the specified angle
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1926
Function: FEATURE_MODEL
Ref: 002-8522825