Show Movable command in Sketcher is not visible in NX

2021-10-06T23:27:50Z

Summary


Details

Show Movable command in Sketcher is not visible in NX 

Solution

To enable the "Show Movable" command in Sketcher go to File > Utilities > Feature Toggles. Under the feature Toggle dialog, Type, "Sketch" and it will filter the "Sketch New SolverAndUI", so change its State from "OFF" to "ON" and click OK.
Refer below snap-





Notes and References

9888154



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: NX
Application: DESIGN
Version: V1930
Function: SKETCHER

Ref: 002-8522702

KB Article ID# PL8522702

Contents

SummaryDetails

Associated Components