Tecnomatix Controllers for ABB, DEFAULT, FANUC, KAWASAKI, KUKA, NACHI, YASKAWA

2021-10-07T00:16:32Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "ABB, DEFAULT, FANUC, KAWASAKI, KUKA, NACHI, YASKAWA" are available for download from https://support.sw.siemens.com.

   See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
   Note: This file is located in the 'OLP Change Logs' folder directly under the
              'Process Simulate Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
   - Scroll down and toggle On the Tecnomatix product.
   - Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate Robot Controllers'
- Select 14.0, 14.0.2, 14.1, 14.1.2, 15.0, 15.0.1, 15.0.2, 15.1, 15.1.1, 15.1.2, 16.0, or 16.0.1

Download the file(s):

    Tecnomatix_14.0_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_14.0_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_14.0_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_14.0_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_14.0_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_14.0_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_14.0_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_14.0_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_14.0_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_14.0.2_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe

    Tecnomatix_14.1_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_14.1_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_14.1_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_14.1_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_14.1_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_14.1_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_14.1_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_14.1_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_14.1_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_14.1.2_ABB_RAPID_64BIT_v3.61.3_19_12_2020.exe
    Tecnomatix_14.1.2_DEFAULT_64BIT_v2.74_19_12_2020.exe
    Tecnomatix_14.1.2_FANUC_RJ_64BIT_v3.3_19_12_2020.exe
    Tecnomatix_14.1.2_FANUC_RJ_JAPAN_64BIT_v2.91_19_12_2020.exe
    Tecnomatix_14.1.2_KAWASAKI_AS_64BIT_v4.8.2_19_12_2020.exe
    Tecnomatix_14.1.2_KUKA_KRC_64BIT_v4.35_19_12_2020.exe
    Tecnomatix_14.1.2_KUKA_KRC_BMW_64BIT_v3.32_19_12_2020.exe
    Tecnomatix_14.1.2_NACHI_SLIM_64BIT_v4.24.4_19_12_2020.exe
    Tecnomatix_14.1.2_YASKAWA_INFORM_64BIT_v5.14_19_12_2020.exe

    Tecnomatix_15.0_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.0_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_15.0_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_15.0_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_15.0_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_15.0_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_15.0_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_15.0_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_15.0_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_15.0.1_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.0.1_DEFAULT_64BIT_v2.74_19_12_2020.exe
    Tecnomatix_15.0.1_FANUC_RJ_64BIT_v3.3_19_12_2020.exe
    Tecnomatix_15.0.1_FANUC_RJ_JAPAN_64BIT_v2.91_19_12_2020.exe
    Tecnomatix_15.0.1_KAWASAKI_AS_64BIT_v4.8.2_19_12_2020.exe
    Tecnomatix_15.0.1_KUKA_KRC_64BIT_v4.35_19_12_2020.exe
    Tecnomatix_15.0.1_KUKA_KRC_BMW_64BIT_v3.32_19_12_2020.exe
    Tecnomatix_15.0.1_NACHI_SLIM_64BIT_v4.24.4_19_12_2020.exe
    Tecnomatix_15.0.1_YASKAWA_INFORM_64BIT_v5.14_19_12_2020.exe

    Tecnomatix_15.0.2_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.0.2_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_15.0.2_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_15.0.2_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_15.0.2_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_15.0.2_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_15.0.2_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_15.0.2_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe

    Tecnomatix_15.1_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.1_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_15.1_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_15.1_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_15.1_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_15.1_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_15.1_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_15.1_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_15.1_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_15.1.1_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.1.1_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_15.1.1_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_15.1.1_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_15.1.1_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_15.1.1_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_15.1.1_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_15.1.1_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_15.1.1_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_15.1.2_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_15.1.2_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_15.1.2_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_15.1.2_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_15.1.2_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_15.1.2_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_15.1.2_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_15.1.2_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_15.1.2_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_16.0_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_16.0_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_16.0_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_16.0_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_16.0_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_16.0_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_16.0_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_16.0_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_16.0_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe

    Tecnomatix_16.0.1_ABB_RAPID_64BIT_v3.61.3_18_12_2020.exe
    Tecnomatix_16.0.1_DEFAULT_64BIT_v2.74_18_12_2020.exe
    Tecnomatix_16.0.1_FANUC_RJ_64BIT_v3.3_18_12_2020.exe
    Tecnomatix_16.0.1_FANUC_RJ_JAPAN_64BIT_v2.91_18_12_2020.exe
    Tecnomatix_16.0.1_KAWASAKI_AS_64BIT_v4.8.2_18_12_2020.exe
    Tecnomatix_16.0.1_KUKA_KRC_64BIT_v4.35_18_12_2020.exe
    Tecnomatix_16.0.1_KUKA_KRC_BMW_64BIT_v3.32_18_12_2020.exe
    Tecnomatix_16.0.1_NACHI_SLIM_64BIT_v4.24.4_18_12_2020.exe
    Tecnomatix_16.0.1_YASKAWA_INFORM_64BIT_v5.14_18_12_2020.exe


To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

SFB-TECNOMATIX-8522666
Product Information:
  • Product: TECNOMATIX , Application: PROCESS_SIMULAT

KB Article ID# PL8522666

Contents

SummaryDetails

Associated Components