NX
About "UGII_CHARACTER_FONT_DEFAULT" environment variable.
2021-10-06T23:27:50Z
NX for Design
Summary
Details
About "UGII_CHARACTER_FONT_DEFAULT" environment variable. How does it work?
Solution
This environment variable UGII_CHARACTER_FONT_DEFAULT is only applicable when the font cannot be found in the defined font folders.
Refer to the below cases for more information.
Case-1
However, user define fonts to use as NX Fonts Only in [Customer Defaults]
and set Standard Font (Arial)" as common text in [Customize Standard]. And Specify UGII_CHARACTER_FONT_DEFAULT as kanji to ugii_env.dat. or set the variable as shown in the image.
It displays the default font as "Kanji". Case-2.
However, users define fonts use as Standard and NX Fonts in [Customer Defaults].
Display default font as "Arial"
Because set Standard Font (Arial)" as common text in [Customize Standard]. Case-3.
However, user define fonts use as NX Fonts Only in [Customer Defaults]
And set NX Font (ideas_kanji)" as common text in [Customize Standard].
Display default font as "ideas_kanji".
Notes and References
9942649
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V1946.4000 Function: ANNOTATION