General Fault Exception - NX Crashes on start-up connected to a Dell Docking

2021-10-06T23:27:50Z

Summary


Details

Normally starting NX on a laptop works just fine, but as soon as the Laptop is plugged in into a Dell Docking (in this case a D3100), NX crashes on Start-up. So unable to start NX.

The error message that pops-up is:

NX Initialization Error

General Fault Exception



The Error in the syslog will show something like this:

*** EXCEPTION: O/S ERROR: signal  11 in line 2888 of o:\nx1926\ip1700\src\syss\error\ind\error.cxx at Wed Nov 11 13:24:43 2020 W. Europe Standard Time
+++ General Fault Exception
+++ Invalid write to 0000000000000000
    rsp:       5a0cdfcc28, rip:                0, rbp:       5a0cdfcd30
    rsi:      247b11209b0, rdi:         40000380
    rax:                0, rbx:      247b10d1dc0, rcx:       5a0cdfcd10, rdx:       5a0cdfcc80
    r8:                5a, r9:                5e, r10:               a2, r11:       5a0cdfc930
    r12:                4, r13:                0, r14:                0, r15:      247b10d1030
[ 1] 000000000000                                                              () 
[ 2] 7FFD379151D2                                                              (ig9icd64) 
[ 3] 7FFD378FD471                                                              (ig9icd64) 
[ 4] 7FFD378EE0B4                                                              (ig9icd64) 
[ 5] 7FFDC82C329B                                                              (OPENGL32) 
[ 6] 7FFDC82C0E1A                                                              (OPENGL32) 
[ 7] 7FFDC82C32FC                                                              (OPENGL32) 
[ 8] 7FFDC82DF4D0                                                              (OPENGL32) 
[ 9] 7FFDC82E04F1                                                              (OPENGL32) 
[10] 7FFDC82DF8F3                                                              (OPENGL32) 
[11] 7FFDE3CD0699                                                              (gdi32full) 
[12] 7FFD42D12952                                                              (libgraphics_driver) 
[13] 7FFD42D11EA2                                                              (libgraphics_driver) 
[14] 7FFD42CF8E88                                                              (libgraphics_driver) 
[15] 7FFD42CE1939                                                              (libgraphics_driver) 
[16] 7FFD42C39600                                                              (libgraphics_driver)



Solution

The issue is somehow Graphics Card related. Most likely because the docking does not properly support the high performance graphics card, but uses the low performance onboard Graphics card.

There are a few ways to see if you can get this resolved.

Most likely one to solve it is:
It was solved by Disabling "Switchable Graphics" in the BIOS. After this all worked fine again.

Downside of this option is that the Nvidia graphics card is used for everything and no longer uses the onboard graphics card. Which may be bad for general laptop performance, battery usage and heating of the laptop. 

Possible other suggestions to try to solve this:


  • Replace the docking/hub by a different model.
  • Start the software without being connected to the docking and reattach the docking after starting NX.
  • Update your graphics drivers, for both Nvidia as well as you Intel UHD onboard graphics.
  • Update the drivers for the (usb) docking
  • Update the Display link drivers (see below for details)
  • Either set the right graphics card in the Nvidia control panel for NX (ugraf.exe)
  • Or set the right graphics card in Windows display settings (right click your desktop --> Display settings --> Graphics settings and add NX here:
Graphics settings:


About the DisplayLink drivers:

You'll find the current version in your windows taskbar.
At the time of writing, there is already a version 10.x available.
 
According to the release notes it's solving quite some display issues for dockings in general.
 
It can be found here:
https://www.displaylink.com/downloads/windows





Hardware/Software Configuration

Platform: na
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1926
Function: WNT_OS_ISSUES

Ref: 002-8522337

KB Article ID# PL8522337

Contents

SummaryDetails

Associated Components