NX
Circular Edges are not accurately visible, display as polygon lines in Assemblies.
2021-10-06T23:27:49Z
NX for Design
Summary
Details
In Native NX1926, circular edges are not displaying correctly, they are displayed as polygonal lines.
Solution
The change in display in the assembly files, is due to the load option "Minimally Load", which is the default load option in NX1926 native NX.So if you select this load option, the display of the components changes to the "Facets/Lightweight" display. To change the display, select all the components in Assembly Navigator and then select the context menu option "Show Exact". The other option to avoid this display is to select a different load option in the Assembly load options dialog. You can select the "Partially Load" or "Fully Load" option to display the exact mode.
Hardware/Software Configuration
Platform: INTEL OS: windows OS Version: 1064 Product: NX Application: ASSEMBLIES Version: V1926 Function: PART_FILE_OPS