Hence the lower limit for the number of teeth for the internal gear cannot be lowered beyond 14.
To avoid a gear interference issue the standard recommendation is there should be at least 15 teeth or more than 15 teeth on the pinion if the pressure angle is 20°.
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: SOLID_EDGE Application: APPLICATION Version: V221MP1 Function: ENGR_REFERENCE