Solid Edge Some docking panes do not behave as expected since Solid Edge 2021 has been installed

2021-10-06T23:57:52Z
PART/SHEETMETAL

Summary


Details

Users will find that the following docking panes do not behave as expected.  They seem not to be docking panes any longer:

YouTube
Requirements
Feature Playback
NX Nastran Log Viewer
Connected Mode Log Viewer



Solution

In version 2021, we addressed many ERs in our docking pane project.  As a part of that project panes that were identified as low usage were converted to panes that could not be docked.  The docking pane system - through years of development - became very complex with the addition of functionality year after year. This change was made to reduce complexity within Solid Edge.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V221.0
Function: UI

Ref: 002-8522119

KB Article ID# PL8522119

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES