NX Changes in Flow Cut to Flow Mill Migration

2023-07-10T17:43:23Z
NX for Manufacturing

Summary


Details

What changes were made when replacing Flow Cut with Flow Mill?

Solution

For Flowcut to FLowMilling the following parameters are migrated:

1.  The Cut Between levels for Zlevel Pattern is removed and turned off on the system level.

2. Max Concavity is removed and will always be 179 degrees.

3. Cross Cut and ZLevel patterns are removed for Non-Steep Cutting

4. Cross cut patterns removed for Steep Cutting Notes

If you set the Customer Default "Automatically Migrate FlowCut Operations" the Flowcut to Flowmill conversion is done automatically. Otherwise, you can do it selectively from the ONT.

Customer Default Automatically Migrate FlowCut Operations

Notes

KB Article ID# PL8521916

Contents

SummaryDetails

Associated Components

Manufacturing General