sketch solver shows still enabled after option turned off.

2021-10-06T23:27:49Z

Summary


Details

After enabling the new 'Sketch_NewSolverAndUI' feature toggle available under File-> Utilities-> Feature Toggle, the new functionality cannot be disabled even if the feature toggle is set to Off. 



Solution

This is working As Designed to assist in migrating forward with the new sketch functionality. 
 Any new sketches in the file will use the new interface and any existing sketches will be given the option to be converted to the new sketch interface even if the feature toggle is set to Off.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ARCHITECTURE
Version: V1926
Function: FEATURE_TOGGLE

Ref: 001-9948737

KB Article ID# PL8521619

Contents

SummaryDetails

Associated Components