After the installation of the Standard Parts Administrator, the guide is installed locally and can be accessed through the Windows Start menu under 'Siemens Solid Edge 2021'.
Standard Parts User Guide
The Standard Parts User Guide will be installed with the Standard Parts Administrator and can then also be accessed through the Windows Start menu under 'Siemens Solid Edge 2021'.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: SOLID_EDGE Application: APPLICATION Version: V221.0 Function: STANDARD_PARTS