Mapping Release status from the ItemRevision

2021-10-06T23:27:49Z

Summary


Details

How to map the release status to the UGPART drawing specification. 
Once this attribute is mapped to the drawing, it can be used as a note on the drawing title block.



Solution

1. Export your Teamcenter mapping file. 
    a. Open a Teamcenter command prompt. 
    b. Type: export_attr_mappings -u=infodba -p=<password> -g=dba -file=C:\user\mapping.txt 
        NOTE: Specify your own infodba password and specify a path for the mapping file that fits your folders. 
2. Edit the mapping.txt in a text editor. 
    a. Under UGPART, add the following mapping: 
        NOTE: That you would enter the ItemType of the data being mapped. This example is mapping to the OOTB "Item" ItemType.


{ Dataset type="UGPART" 
 # (hard-wired) DB_DATASET_ID : "Part File ID" 
 # (hard-wired) DB_DATASET_REV : "Part File Rev" 
{Item type="Item" 
RELEASE_STATUS_NAME : ItemRevision.last_release_status.name /allow_null_value /master=iman /description="Release Status Name" 

}


3. Save the mapping file. 
4. Import the modified mapping file back into Teamcenter. 
    a. Open a Teamcenter command prompt. 
    b. Type: import_attr_mappings -u=infodba -p=<password> -g=dba -file=C:\user\mapping.txt 
        NOTE: Specify your own infodba password and specify a path for the file that fits your folders.

Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: ATTRIBUTES

Ref: 001-9945865

KB Article ID# PL8521331

Contents

SummaryDetails

Associated Components