NX Release Update is available for download

2025-03-25T23:34:14Z

Summary


Details

Dear Siemens Customer,   

We are pleased to inform you that the latest product release of NX is now available for download from the Siemens Digital Industries Software Support Center      

Please use the following steps to download the NX product release and its documentation.  

Note: A valid WebKey account is required.        

  • In your browser's address field enter the URL: https://support.sw.siemens.com/en-US/product/209349590/downloads   
    • Login using your WebKey username and password      
      • From the Support Center page, select “NX 2412 Series” from the Version dropdown. Then select "NX 2412.5000" from the Release tiles to return the list of links for the Release Letter and the Release Packages.   

        Click on the Release Package files to download the NX product.    

          Download of NX on Windows 64-bit      

        • Note: There are two options to download NX. The first option is recommended for customers running the most recent versions of NX. To upgrade, download the following file and double click to begin the installation program. Automatic updates are currently available.   
          • SiemensNX-2412.5001_wntx64_MSP.zip      
            • The second option is recommended for customers who do not have a previous NX Series release installed.   
              • SiemensNX-2412.5001_wntx64.zip

                Download of NX Batch on Linux 64-bit

                • Download the following file and double click to begin the installation program:  
                  • nxbatch_2412.5001_lnx64.tar.gz    
                    • Extract the tar.gz with:     
                      • cat nxbatch_2412.5001_lnx64.tar.gz | gunzip | tar -xvf  
                        • Run the install from inside the location to which the tar.gz file was extracted:    
                          •  ./run_install

                            Please refer to the readme file with the download for instructions on extracting the main zip file.   

                            • NX Release Notes can be found in the downloads area along with the zip files

                              In all cases, please refer to the supplied README file for installation instructions.       

                              If you encounter any problems during this installation, please contact your local Siemens Digital Industries Software support office.      

                              For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:     

                                         https://www.plm.automation.siemens.com/global/en/products/nx/

                                         https://support.sw.siemens.com

                              Sincerely
                              Siemens Digital Industries Software

                              KB Article ID# PL8838680

                              Contents

                              SummaryDetails

                              Associated Components