Solid Edge
Where to find the programming examples for Solid Edge
2021-10-06T23:57:49Z
PART/SHEETMETAL
Summary
Details
When trying to create Add Ons for Solid Edge by programming, it is often very helpful to use the programming examples that can be found in the Custom Directory below the Solid Edge Folder:
In each Directory one can find Visual Studio Solutions with programming code.
This has changed now with Solid Edge 2021:
So where are the useful programming examples ?
Solution
Since Solid Edge 2021 the Custom directory has been removed.
However, the examples are still available in Support Center:
You will find them below the Solid Edge 2021 Add-ons:
The Zip file contains the complete Directory with all available Examples:
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: n/a Product: SOLID_EDGE Application: SETUP Version: V221.0 Function: INSTALL