SIMIT MCD Add-in toolbar failed to show after upgrade of NX.
2021-10-06T23:27:49Z
Summary
Details
After upgrade of NX, the toolbar for the SIMIT add-in does not show anymore. This SIMIT plug-in is part of the SIMIT 10.2 install.
Solution
There are 2 options:
1) Reinstall the SIMIT MCD Add-in via the SIMIT installer; 2) or Manually repair the custom_dirs.dat: You best check chapter 3 in "Installation Guide SIMIT MCD Add-in.pdf"
Manual setup of the SIMIT MCD Add-in
3.1 Target directory of the SIMIT MCD Add-in
During the installation of SIMIT all necessary files for the SIMIT MCD Add-in are stored by default in the following target directory:
The files are stored regardless of whether your system settings meet the above- mentioned requirements for an automatic installation.
3.2 Settings at Custom_dirs.dat von SIEMENS NX
3.2.1 Check the target directory for custom_dirs.dat.
SIEMENS NX manages the extensions used in the configuration file custom_dirs.dat. In the standard installation case, the file is in the following directory:
C:\Programs\Siemens\NX1899\UGII\menus
Please note that this directory structure may differ depending on your SIEMENS NX version. Using the environment variable UGII_CUSTOM_DIRECTORY_FILE you can adjust the target directory for the custom_dirs.dat file to your requirements. You should therefore check in your system settings which target directory is referenced for the configuration file custom_dirs.dat.
3.2.2 Extending the configuration file Custom_dirs.dat for the SIMIT MCD Add-in
To enable SIEMENS NX to use the SIMIT MCD Add-in, it must be entered in the configuration file custom_dirs.dat. Open this configuration file in the correct target directory of your system settings and add the path specification that refers to the storage directory of the SIMIT MCD Add-in at the end of the file. In standard installation case add the following entry: