Solid Edge SEEC error on revise ItemRevision when object_desc is required

2021-10-06T23:57:49Z
DOC_MANAGEMENT

Summary


Details

The customer has set the ItemRevision.object_desc to required in the BMIDE. 
They want to revise a released Item Revision with SEEC but this will fail with the error: Cannot Checkout <file name> because it is released or you do not have permissions to check it out.


Steps to reproduce:


- Create a SE part and save to Teamcenter 
- Save and close the SE part 
- Release the Item Revisions and SE part 
- Open in SEEC (read only) 
- Revise 
- Perform action in the CPD will give the Cannot checkout error 







Solution

In the CPD we do not honor the Revise descriptor in a Revise case. 

The workaround is:


- remove the required flag in the BMIDE 
- Make an attribute mapping to ItemRevision.object_desc with the qualifier /required


The result is the same: in the CPD the object_desc is marked as required, but the Revision is not blocked 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-9933782

KB Article ID# PL8520813

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC