Details
You have customized your proseed.txt and added language specific characters (eg. Russian or German) which are not displayed correctly in the custom properties menu inside Solid Edge. Why?
Solution
There are two possible reasons for this:
1.
We deliver propseed.txt in non-English installations in simple text format, but if special characters are included that needs to be saved using UTF-8 format. You can simply do a 'save as' and select encoding 'UTF-8' at the bottom of the 'save as'-menu.
2.
Ensure you have MP1 for Solid Edge 2021 installed. Only with MP1 are those special characters from propseed.txt supported in Solid Edge 2021.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V221MP1
Function: PROPERTIES
Ref: 002-8520706