Modify Shortcuts popup on features to include or exclude commands
2021-10-06T23:27:49Z
Summary
Details
Comparing the Right Mouse Button shortcut popup over Features in Part Navigator between NX1926 and previous NX releases, noticed NX 1926 has minimum commands shown:How to customize this shortcut popup for features in Part Navigator to include/exclude commands?
Solution
(1) Go into the Customize mode ("menu > Tools > Customize..." or "Ctrl = 1") (2) In the Customized dialog, go to the Shortcuts tab (3) Highlight "All Features" (the 3rd line on the list) (4) Notice the shortcut popup that appears on the screen:(5) Go to the Commands tab, expand "Menu > Edit", find and highlight "Feature". (6) On the right side column "Items", scroll and find "Make Current Feature" (as an example), select it and hold and drag/drop it in that empty shortcut popup from step(4) (7) Close the Customize dialog and you have successfully customized that shortcut popup to include the "Make Current Feature".
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: SYSENG Version: V1926 Function: UI_TOOLS