Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that the Tecnomatix Plant Simulation Maintenance Pack V16.0.1 is available for download from the Siemens Digital Industries Software Support Center.
Note: A valid WebKey account is required.
Please use the following steps to download the maintenance pack:
In your browser's address field enter the URL: https://support.sw.siemens.com/product/297028302/downloads
Login using your WebKey username and password
From the Support Center page, select "Plant Simulation 16" from the Version drop-down list. Then click on the tile "Plant Simulation 16.0 Maintenance Packs". In the list on the left side click on the language "English" or "Deutsch", and then on "MP01" to show the files to download.
To install:
Place the file
PlantSimulation16.0.1.MaintenancePack.exe into a folder.
Execute PlantSimulation16.0.1.MaintenancePack.exe.
The patch will automatically detect the installation folder.
If you encounter any problems during this installation, please contact your local Siemens Digital Industries Software support office.
Sincerely,
Siemens Digital Industries Software
SFB-TECNOMATIX-8520090
Product Information:
- Product: TECNOMATIX , Application: PLANTSIMULATION , Version: V16.0