Endpoints in Sketch do not stay coincident

2021-10-06T23:27:49Z

Summary


Details

When using the 'Rectangle' command in a sketch, the endpoints of the lines do not stay coincident if the rectangle is re-sized. 
1. In a Sketch, select the 'Rectangle' icon. 
2. Draw a rectangle and complete the operation. 
3. Select one of the endpoints in one of the corners of the rectangle. 
4. Drag and move the end point to resize the rectangle. 
Only the line is resized and the line is no longer connected to the rectangle. 
The endpoints of the lines in the rectangle should have been automatically constrained to be coincident so when one endpoint is moved, the endpoints of the other lines are also moved.



Solution

1. While in the Sketch, select in the Menu, 'Task-->Sketch Settings'. 
2. Toggle ON 'Create Inferred Constraints'. 
3. OK the Sketch Settings dialog. 
4. In the Menu, select 'Tools-->Constraints-->Inferred Constraints and Dimensions'. 
5. Toggle ON 'Coincident'. 
6. OK the Inferred Constraints and Dimensions dialog. 
Now when a rectangle is created and one of the corners is moved, the entire rectangle should be re-sized instead of just moving that endpoint.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1953
Function: SKETCHER

Ref: 001-9931383

KB Article ID# PL8519821

Contents

SummaryDetails

Associated Components