When a Master is a component of a drawing file, how can you import the drawing file such that it will exist under the Master?

Solution
Import Assembly into Teamcenter --> Select Assemblies or Parts --> select the drawing file --> OK.
In the dialog, set the drawing Relation Type to Specification:

Set the Dataset Name:

Double-clicking will use the Object name:
Set a Default Destination Folder and OK:

If the component already exists in the Teamcenter database, set the following in the dialog prior to OK:

Hardware/Software Configuration
Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1946
Function: CLONE_IMPORT
Ref: 002-8519260