Objects are visually hidden in NX while rotating the model

2021-10-06T23:27:48Z

Summary


Details

After opening a part, a body is always cut off after rotating the body and is not displayed correctly.



Solution

The first possibility would be to refresh the display via FIT (MB3). This brings the components back into the screen space.

In this Example: Right Window is wrong - Left Window is corecct after FIT.


But after saving it can happen that the behavior occurs again. Then the next step is to check and change the camera positions in the ANT and to modify the Cameras.

Go to part navigator and edit the "Trimetric" Camera. It will show the view clipping plane defined on the edge of the solid for this example.

NX will show objects inside the clipping planes, so when you rotate, a part of the solid will be clipped and hidden.

Fit view will recalculate the default clipping plane distances based on the defined objects, you can observe the view clipping by view information.

Example:
Front Z-Clipping     =     568 mm
Back Z-Clipping      =    -568 mm
Hence, for the part, user defined the camera, then save the part directly, so NX following camera clipping definition behavior on the view.
(Fit Planes to Extents)



After the clipping plane has been changed and the camera positions is saved, the behavior should be normal again.






Notes and References

Thanks  Jackie Zhang

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1942
Function: GRAPHICS

Ref: 002-8519252

KB Article ID# PL8519252

Contents

SummaryDetails

Associated Components