Solid Edge Solid Edge cloud licensing with Remote Desktop

2024-08-05T05:30:17Z
PART/SHEETMETAL SETUP

Summary


Details

The traditional Solid Edge node locked licensing model does not support running Solid Edge through a Remote Desktop Session.  If the node locked license is converted to use cloud licensing, will Solid Edge run through a Remote Desktop session if cloud licensing is enabled?

Solution

Yes, Solid Edge with cloud enabled licensing will allow Solid Edge to run through a Remote Desktop environment.

Notes

If you have further inquiries about Cloud Licensing please refer to the FAQs collection link below:

Solid Edge Cloud License FAQs Collection


KB Article ID# PL8519251

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES