How do you set snap angle for view sectioning in NX session.

2021-10-06T23:27:48Z

Summary


Details

While doing View Sectioning in Modeling and you would like to set the snap angle, you can do the following:



Solution

 Edit Section --> From the dynamic WCS --> Select the ball for the rotation handle (left mouse click) on an axis to bring up the Angle and Snap then enter the desired values -> Hit Enter then the snap angle stays for the session.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1892.4100
Function: GRAPHICS

Ref: 001-9923954

KB Article ID# PL8519158

Contents

SummaryDetails

Associated Components