Exporting a JT of an assembly to include PMI to import back into NX
2021-10-06T23:27:48Z
Summary
Details
If you have PMI created at the component level and being pushed to a higher assembly level using PMI Assembly Filters, how can you export JT and import it back to NX that includes the PMI?
Solution
NX does not support PMI Assembly Filters in Monolithic JT assemblies, so you would need to use "As Assembly and Folder of Parts" option when exporting JT of NX assemblies with PMI Filters. Then open the JT assembly using either partial or fully load. Lightweight load options won't load enough data.
Notes and References
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: PMI Version: V1930 Function: JT_INPUT