PLM Open JT2Go cannot open Solid Edge 2021 files

2021-10-06T23:57:39Z
PLM Components

Summary


Details

JT2Go cannot open files created in Solid Edge 2021 and an error message is displayed:

The PLMXML document could not be loaded!


Solution

The current version of JT2Go does not have the latest PLMXML adapter required for reading Solid Edge 2021 files. This is because JT2Go was released BEFORE Solid Edge 2021. Hence you will get a PLMXML error when opening Solid Edge 2021 files:

In order to overcome this you will need to install the latest PLMXML adapter for SE2021 in to the JT2Go program files.

From Support Center locate and download the Solid Edge 2021 PLMXML files:

https://support.sw.siemens.com/en-US/downloads/PL20200727101459570/akamai?uri=https%3A%2F%2Fdownloada.industrysoftware.automation.siemens.com%2Fsc_downloads_prod%2Fb%2Ff%2F9c35451d7b68a27bc6d3cc840543fa%2FV221_PLMXML_FILES.zip


From the downloaded zip file extract the plmxmlAdapterSE70.dll file and replace the existing file in the "C:\Program Files\Siemens\JT2Go\Program" folder. You may want to back up the original plmxmlAdapterSE70.dll first:

Now JT2Go will read Solid Edge 2021 files without issue:




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V221.0
Function: PLMXML
Product: PLM_OPEN
Application: JT2GO
Version: V13.0.0
Function: JT2GO

Ref: 002-8519048

KB Article ID# PL8519048

Contents

SummaryDetails

Associated Components

JT2GO JT2GO_JTOE