NX
Connection OPC-DA to SIMATIC NET: symbols with forward-slash " / " are not recognized.
2021-10-06T23:27:48Z
NX for Design
Summary
Details
When connecting SIMATIC NET / TESP 7 to NX MCD using OPC DA server, then all symbols in STEP 7 which contain a forward slash " / " in the name, are not recognized by NX (in External Signal Configuration dialog).
STEP 7 example of unrecognized symbol name:
Solution
Do not use a forward slash in the symbol names. It will just not be recognized in NX MCD as Tag in External Signal Configuration and Signal Mapping. Currently (NX 1926 series), MCD use a " / " as separator of the path.
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: MECHATRONICS Version: V1926 Function: SIGNAL